ECADEMY

About pump curves

Pumps_Task 04_main image_900x425

About pump curves

The performance of a centrifugal pump is shown by a set of performance curves. The performance curves for a centrifugal pump are shown in figure 1. Head, power consumption, efficiency and NPSH are shown as a function of the flow.


Fig. 1: Typical performance curves for a centrifugal pump. Head, power consumption, efficiency and NPSH are shown as a function of the flow

Normally, pump curves in data booklets only cover the pump part. Because of this, power consumption, the P2-value, listed in data booklets, only covers power going into the pump (see figure 1). The same goes for the efficiency value, which only covers the pump part (η = ηP). In some pump types with integrated motor and perhaps also an integrated frequency converter, e.g., canned motor pumps, the power consumption curve and the η-curve cover both the motor and the pump. In this case it is the P1-value that has to be taken into account.

In general, pump curves are designed according to ISO 9906 Annex A, which specifies the tolerances of the curves:

• Q +/- 9%,

• H +/-7%,

• P +9%

• η-7%.

Fig. 2: The curves for power consumption and efficiency will normally only cover the pump part of the unit – i.e.,P2 and ηP.

What follows is a brief presentation of the different pump performance curves.

Head, the QH-curve
The QH-curve shows the head the pump is able to perform at a given flow. Head is measured in meter liquid column [mLC]; normally the unit metre [m] is applied. The advantage of using the unit [m] as the unit of measurement for a pump’s head is that the QH-curve is not affected by the type of liquid the pump has to handle.

Fig. 3: A typical QH-curve for a centrifugal pump; low flow results in high head and high flow results in low head.

Efficiency, the η-curve
Efficiency is the relation between power supplied and the amount of power actually utilised. In the world of pumps, the efficiency ηP is the relation between the power the pump delivers to the water (PH) and the power input to the shaft (P2 ):

where:

ρ is the density of the liquid in kg/m3,
g is the acceleration of gravity in m/s2,
Q is the flow in m3/h and H is the head in m.

For water at 20°C and with Q measured in m3/h and H in m, the hydraulic power can be calculated as:

As it appears from the efficiency curve, efficiency depends on the pump’s duty point. This makes it important to select a pump that fits the flow requirements and ensures that the pump is working in the most efficient flow area.

Power consumption, the P2-curve
The relation between a pump’s power consumption and flow is shown in figure 5. The P2-curve of most centrifugal pumps is similar to the one in figure 5, where the P2 value increases when flow increases.

NPSH-curve (Net Positive Suction Head)
The NPSH-value of a pump is the minimum absolute pressure that must be present at the suction side of the pump to avoid cavitation. NPSH-values are measured in [m] and depend on flow; when flow increases, the NPSH-value also increases (see figure 6).

..PDF

Pumps_Task 4_About pump curves.pdf (size: 0.1MB)

ΣΩΣΤΕ ΤΟ ΑΡΧΕΙΟ